When an input signal containing interference waves is input into a non-linear system, the frequency component (intermodulation product) generated by the linear combination of the frequency contained in the input signal will be included in the output signal.
Sufficient measures must be taken concerning the generation of one of the third-order intermodulation components 2𝑓1−𝑓2 in the passband, which leads to remarkable deterioration of the communication quality.